11/8/2013 8:25 AM | |
Posts: 1368 Rating:
|
Hello Red Alert, the easiest way i think is the open communication with the t-blocks TCON, TSEND/TRCV and TDISCON. Information for the open communication you find here http://support.automation.siemens.com/WW/view/en/78028908 http://support.automation.siemens.com/WW/view/en/29737950 Good luck, Pittiplatsch |
This contribution was helpful to
1 thankful Users |
11/12/2013 9:55 AM | |
Posts: 23 Rating:
|
Dear Pittiplatsch& all Experts, |
11/12/2013 10:09 AM | |
Posts: 1368 Rating:
|
Hello Red Alert, the second link http://support.automation.siemens.com/WW/view/en/29737950 decribes, which blocks are necessarry and how to configure them. TCON is responsable to build up the connection. TSEND / TRCV are responsable for sending/receiving data TDISCON disconnect the connection. Additionally there are 2 data blocks for the information IP address, ports, type of connection etc. Information you also find in the help sites of TIA. It is easy to configure...no problem.... |
12/7/2015 11:14 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4766 Rating:
|
New question published by Glenn@CNCDesign is split to a separate thread with the subject Receive Data blocks via Profinet. Best regards |
9/28/2016 2:56 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4766 Rating:
|
New question published by M__G is split to a separate thread with the subject Hardware configuration CPU 414-5H and CPU 313C Via CP343-1 Lean. Best regards |
Follow us on