8/18/2009 12:22 PM | |
Posts: 61 Rating: (0) |
Dear all, used WLAN client is W744-1 Pro. used conenction type is S7 Connection ( NetPro). attached is the IP address details for all component used. kindly suggest the possible silution. one thing, my all ES, SERVER1, SERVER2 and PC station are able to ping the PLC simultaneously. worry is : all are not going online simultaneously????? AttachmentBorouge Network Setup.pdf (126 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on