3/3/2021 7:46 PM | |
Joined: 2/6/2015 Last visit: 4/4/2025 Posts: 80 Rating:
|
Hi wrc286ralli, On SIOS you will find information for configuration the first steps between a HMI and a PLC as S7-1200. At this link it described as configure the connection: https://support.industry.siemens.com/cs/ww/es/view/109773787/69470254603?dl=en and this other link a basic application example: https://support.industry.siemens.com/cs/ww/es/view/54430386/39281800203?dl=en |
If this Information really helps, you could use the Rate function |
|
3/4/2021 6:55 AM | |
Posts: 2 Rating:
|
Thanks for the reply. I am familiar with the general information of working with the portal But I did not find such a solution. -I have a wincc station and need to get tags from the plc that are located on the equipment. I don't have a plc project! The wincc station and the plc have the same subnet . I attach a photo. AttachmentScreenshots.zip (89 Downloads) |
Last edited by: Jen_Moderator at: 03/04/2021 07:46:42Added all files as a zip file. |
|
3/4/2021 5:26 PM | |
Joined: 2/6/2015 Last visit: 4/4/2025 Posts: 80 Rating:
|
Hi wec286ralli, If you don't have a PLC integrated in the project you should configure the tags as absolut address. By example: DB1.DBW0 Another option is to use "PLC Proxy". In this way you would have the tags accessible in the WinCC project Combined configuration with WinCC (TIA Portal) and STEP 7 V5.x or Combined configuration with WinCC (TIA Portal) and STEP 7 (TIA Portel) in separate projects (Video) https://support.industry.siemens.com/cs/cr/es/view/73502293/en |
If this Information really helps, you could use the Rate function |
|
Follow us on