7/23/2015 10:44 AM | |
Posts: 4 Rating:
|
Hello,
Now I have 64KB memory card and my project uses 94% of load memory, but I can't transfer project changes to PLC, because I get error, that where is not enough space. I tried to load empty project to PLC, but in online monitoring I saw that 14% of load memory is still used. Can somebody explain me this and tell if it is possible to reset load memory?
|
7/24/2015 1:55 AM | |
Joined: 9/27/2006 Last visit: 4/4/2025 Posts: 12345 Rating:
|
Hello Mn; You could start by reading the following document, and look at the available links, to have a general idea of the way memory is structured in a S7-300 CPU, and distinguish load and work memory areas: How can you obtain an overview of the memory concept of SIMATIC S7-300 CPUs and C7 devices? Your situation will depend on the exact part number (MLFB) of your CPU, depending on the age of the CPU it will use either a MC (RAM or EPROM) or a MMC as load memory. As a rule of thumb, the ration of load to work memory should be at minimum 1 to 1:5. That is a 64 kB memory card would be adequate for a CPU having 48 kB work memory; only very old S&-300s have that small a work memory. So please provide the MLFB of the CPU you want to use so we can help out. I would also be useful if you attach a screenshot of your memory settings, from the CPU properties, in HWConfig (runtime), and the type and size of the presently used memory card. Hope this helps, Daniel Chartier |
This contribution was helpful to
3 thankful Users |
7/27/2015 10:14 AM | |
Posts: 4 Rating:
|
Hello, Daniel,
|
We are working on a new user interface with better overview and more relevance.
To explore the new Forum, you can follow the textbox in the right column, which will lead you to the corresponding page in the new Forum. Alternatively, you can start from the main page by following this link:
https://sieportal.siemens.com/en-ww/support/forum
In the coming days, we will update the configuration step by step, so that you are directed to the new Forum by default. The “classic Forum” will remain available for all known functionalities alongside the new one.
We are thrilled to finally share the future of our Forum with you. Thank you for your commitment!
Kind regards,
the Forum Support Team
Follow us on