1/23/2015 2:11 PM | |
Posts: 3 Rating: (0) |
Can I use PLC Open blocks for position control of G120? Connection betweenS7-1200 and G120 is done by Profinet.G120 is connected to motor and encoder. |
2/6/2015 10:18 AM | |
Posts: 9 Rating: (5) |
Sorry, I see... I think, the best and easiest way is to buy a new S7-1200 controller for this project, like S7-1212 DC/DC/DC(6ES7212-1AE40-0XB0). Fact is, you need firmware version V4.1 for using S7-1200 with motion control over PROFInet connection. You find the firmware at the following link: https://support.industry.siemens.com/cs/de/en/view/106200276 Hope this post will help... |
2/12/2015 9:12 AM | |
Posts: 9 Rating: (5) |
Yes, that's right. You find more information about the function block "SINA_POS" at the following links:
SINAMICS Startdrive https://support.industry.siemens.com/cs/ww/en/view/68034568 In the document "SINAMICS_blocks_TIAP.pdf"
I hope, this info would help... |
5/19/2015 11:55 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4772 Rating: (123) |
|