Industry Online Support
Technical Forum
9/1/2013 1:41 PM | |
Joined: 9/27/2006 Last visit: 1/20/2025 Posts: 12330 Rating: (2700) |
Hello raja; Have a look at the following discussion on ABB drives and S7-1200 PLCs. Our friend Glinglin offersa sample TIA Portalprogram with ACS550 controlsthat might help you out. connect 3 ABB drives ACS550 to an Profibus Master in S7-1200 Hope this helps, Daniel Chartier |
9/2/2013 4:58 AM | |
Posts: 2 Rating: (0) |
hi Daniel Chartier its acs550, but i am using acs-800 the address are different please give me solution how to run via profibus thanks br raja.p |
9/2/2013 3:35 PM | |
Joined: 9/27/2006 Last visit: 1/20/2025 Posts: 12330 Rating: (2700) |
Hello raja; Both ABB dive models use the RPBA Profibus-DP module, so what address is different? See if the links in the following discussion can help: /tf/WW/en/Posts/82332 If not , share your code and configurations, it is extremely difficult to find out what is wrong with so little information on faults and error codes. Hope this helps, Daniel Chartier |
9/3/2013 8:20 AM | |
Joined: 4/21/2006 Last visit: 1/14/2025 Posts: 510 Rating: (24) |
New question was splitted to a new thread: Communication profibus: motoman |
Follow us on