7/18/2006 9:38 AM | |
Posts: 433 Rating:
|
Hello CSI-Group, it is possible to simulate only 1 PLC with PLCSIM. => Unfortunately a comunication between 2 PLCs is not possible. [:cry:] Regards Tomcat |
7/20/2006 8:09 PM | |
Posts: 85 Rating:
|
Oops....... A little bit of Googling....."S7WSPSMX.OCX " is the ActiveX control you need to add. I was looking for DLL but its an OCX. Nevermind. |
7/20/2006 9:56 PM | |
Joined: 1/7/2006 Last visit: 7/3/2023 Posts: 2705 Rating:
|
Hi Waterboy (are you a swimmer [:)]), There is also a nice FAQ: Inserting control element "S7ProSim Control" in Visual Basicand two handbooks where everything about this feature is written: S7ProSim V5.3 incl. SP1 ActiveX Controland S7ProSim V5.3 incl. SP1 COM Object[;)] I have seen also some example of this software, if you want to see it, let it me know and then i search to it.. [8)] |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
Follow us on