10/6/2020 12:40 PM | |
Posts: 55 Rating: (0) |
Hi all, Is it possible to access CPU webserver page remotely without VPN connection (such as using VPN router)? Many Thanks Mido. |
10/6/2020 6:39 PM | ||||
Joined: 3/28/2015 Last visit: 1/24/2025 Posts: 722 Rating: (214) |
Hello,
Perhaps the following points might help: 1-Enable the web server on the CPU 2-Port forwarding in the router setting"Remote side":
"CPU IP Address" If the data is transferred via routers or if firewalls are used, the port must be enabled in the router or firewall according to the service implemented. 3-Office PC"Local side": http://public IP Address:XXXX or http://domain:XXXX |
|||
Eng.Mohamed Ibrahim |
||||
This contribution was helpful to2 thankful Users |
Follow us on