4/21/2018 8:41 AM | |
Posts: 67 Rating: (7) |
Thats not the full version of the manual, there's no or little programming info. On page 50 (52 in the PDF), it looks like input 16, 17 and 18 can be used for speed-reference. My best guess is, that you program them in parameter 3-15, 3-16 and 3-17 (Page 59) Try to find the complete programming manual, it will tell what can be enabled and where to do it. EDIT: Choose the FC302 in the pull down, and tick programming guide in document type, you will find this; "VLT® Automation Drive FC 300 SW 7.62/8.1" On page 68, the speed input reference is mentioned. |
Last edited by: cs_dk at: 4/21/2018 8:53:50 AM |
|
This contribution was helpful to1 thankful Users |
4/27/2018 9:06 AM | |
Posts: 67 Rating: (7) |
I don't know why the links would not work. They work fine here (Firefox). However, I uploaded it HERE Attachment4cfad1b980b4b85b758b6e0d32f23ef0.pdf (227 Downloads) |
Last edited by: cs_dk at: 4/27/2018 9:07:29 AMLast edited by: Jen_Moderator at: 4/27/2018 1:01:12 PMAdded file as an attachment. |
|
Follow us on