10/14/2009 9:03 AM | |
Joined: 4/5/2006 Last visit: 4/23/2025 Posts: 917 Rating:
|
Hi Delphoe , not to understand your trouble...do you have PLCCIM icon available in Simatic Manager? if no, just install it from PCS7 DVD installation bwrowse it to find Plcsim folder and runt installation setup. if you have PLCSIM icon available, just remeber you have to use "PC internal local" connection in Simatic Net Console (in this way when opening plcsim automatically will be changed connection to use it). The other thing is the only connection available for plccim are MPI and Ethernet, so compile OS selecting connection MPI or Ethernet to use WinCC. Regards |
Follow us on