1/16/2015 3:22 PM | |
Posts: 5 Rating: (0) |
Hello, I followed the procedure and I have installed these packages: - TIA Professional V13 SP1 - WinCC Comfort V13 SP1 - Startdrive V13SP1 Note: I've a license for STEP 7 Professional V13 Everything work properly. Instead I have a problem with PLCSIM V13 SP1. When I try to simulate the CPU1200 appears a error message. (Please see attached file). I tried to install PLC SIM V13 SP1 before as stand alone program and after as upgrade of PLCSIM V13 but the error is always the same. Thank you for your support Costantino ------------ New subject after splitting from TIP: STEP7 V13 SP1 and simulation for S7-1200 V4.0 and higher. |
Last edited by: Min_Moderator at: 1/19/2015 12:00 PMSplitted |
|
1/19/2015 3:24 PM | |
Joined: 2/19/2013 Last visit: 3/15/2024 Posts: 184 Rating: (8) |
Strange...Have you try to repair Tia Portal instalation? |
1/19/2015 3:49 PM | |
Posts: 5 Rating: (0) |
I've just update TIA Portal V13 to SP1. Please see attached file. |
1/21/2015 3:53 PM | |
Posts: 5 Rating: (0) |
Thank you a.k, you're right. I installed all the programs on PC with Windows 7 64bit and everything work properly. |
2/20/2017 9:22 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4774 Rating: (123) |
New question published by mohammed yousif is split to a separate thread with the subject Error when installing PLCSIM V13 Update 1. Best regards |
Follow us on