3/7/2016 4:08 PM | |
Joined: 5/7/2015 Last visit: 9/20/2023 Posts: 56 Rating:
|
I'm using S7-1500 with in-rack CM PtP RS485/422 HF as Master. I have only 1 slave. Modbus on RS-485 with 9600 baud, None parity, 8 bits + 1 stop bit.. I wish to have a simple reliable communication with this slave. I have used the example program given in http://support.automation.siemens.com/WW/view/en/68202723 but I have not got useful results. This program works well for a while 2-3 hours and then comes up with various errors such as 81EA, 81E9 etc.. I have checked the slave end (Precia-Molen load-cell controller) and at that end it seems OK. I wish to have a simple single-slave example using the basic instructions so that I can understand and get it to work reliably. Thanks for looking in. |
Follow us on