5/10/2008 1:08 PM | |
Joined: 1/7/2006 Last visit: 2/16/2023 Posts: 2705 Rating:
|
Hi, When the CPU is not in STEP7 then you need a HSP, when the version of your STEP7 is V5.2 or higher then you may import new S7 equipment in the hardware configuration. See the url: Hardware Support Packages (HSPs - 02/2008) It could be that your STEP7 version is to old, read the minimal version in the pdf that is also under the same url. Only PROFIBUS DP CPUs have a GSD-file when they have to be used as a PROIBUS DP Slave. |
I hope that the answer will help, if you have still questions, don't hesitate to ask me. |
|
7/2/2015 12:33 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4812 Rating:
|
|
Follow us on