Industry Online Support
Technical Forum
9/27/2011 9:46 PM | |
Posts: 6 Rating: (0) |
Can u please help me by giving the explanation of all specification terms used in circuit breakers.... This is urgently required for me. Thanks in advance Regards, Prasenjit Roy. Splitted from Distinction between mpcb, mccb, mcb . |
Last edited by: O_Moderator at: 9/28/2011 10:52 AMnew subject after splitting |
|
9/22/2014 8:32 AM | |
Posts: 56 Rating: (2) |
Making and Breaking Capacity of a circuit breaker Making capacity of a circuit breaker is the maximum current which the breaker can conduct at the instant of closing. The making capacity is considered to the peak value of the first cycle when there is an imaginary short circuit between the phases.
When there is a short circuit in the line and the breaker is closed, the peak value of the first cycle is the most severe from an electrodynamic perspective. This value is in kA. The making capacity is expressed as a peak value as the dc offset during fault conditions is taken into account. Breaking capacity of the circuit breaker refers to the maximum current in rms value the circuit breaker can interrupt. This is also in the order of kA. The making capacity of the circuit breaker is usually greater than the breaking capacity of a circuit breaker as breaking an electric circuit is difficult due to arcing which occurs and which has to be quenched. |
9/22/2014 8:33 AM | |
Posts: 56 Rating: (2) |
please specifically ask what is the doubt |
Follow us on