4/29/2012 2:37 PM | |
Posts: 1064 Rating: (72) |
here you go try using the search button and you will find what you need http://support.automation.siemens.com/WW/view/en/59613127 |
4/29/2012 4:24 PM | |
Joined: 4/19/2008 Last visit: 2/9/2024 Posts: 1525 Rating: (159) |
Hello playerlight, You have given a Link of SIMATIC PCS 7/OPEN OS V7.1.3 Update 2which is Migration Tool, Here is the Detail Update of SIMATIC PCS 7 V7.1, V7.1 + SP1 or V7.1 + SP2 to V7.1 + SP3 The existing SIMATIC PCS 7 V7.1, V7.1 + SP1 or V7.1 + SP2 software can be updated to V7.1 + SP3 with the SIMATIC PCS 7 Software Media Package V7.1 + SP3 (data carrier package without license).
to Update You have to pay The L price for the SIMATIC PCS 7 Software Media Packages is 50,00€ in each case. The L price for the SIMATIC PCS 7 Update Package Engineering V7.1 + SP1 to V7.1 + SP2 is 25,00 €. Please note that additional freight and customs charges may become applicable. Have Look on this Link for More Detail. |
Ammy |
|
4/29/2012 5:10 PM |
|
Posts: 1064 Rating: (72) |
Sorry I guess i should look harder when half asleep |
4/29/2012 6:22 PM |
|
Posts: 1064 Rating: (72) |
where i work there are 17 control engineers on day shift and myself on the offshift ,so i think i do pretty good by myself |
4/30/2012 6:35 PM | |
Posts: 34 Rating: (0) |
Thank you so much playersight & Ammy for your help. |