6/21/2010 1:01 PM | |
Joined: 4/19/2008 Last visit: 11/21/2024 Posts: 1525 Rating:
|
Hi UMENCHO, Please tell me in both GET & PUT block what I have to Assine at ADDR_1 if I have to do the communication with S7-200 PLC, I have checked the GET & PUT Example also But it was not providing clear Idea about the S7-200 Mamory is there any CPU Version Issue for this Block ??? Splitted from Ethernet comunication between Siemes S300 - S200. |
Last edited by: O_Moderator at: 6/22/2010 12:39 PMnew subject after splitting Ammy |
|
6/21/2010 4:14 PM | |
Joined: 4/19/2008 Last visit: 11/21/2024 Posts: 1525 Rating:
|
Hi, I have done the Communication with exiting backup & GET & PUT logic given in FAQ with address related to Example given in the communication PDF. |
Ammy |
|
Follow us on