2/29/2016 8:33 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating:
|
hi sk-singh, Do you use TIA or the classic Step7 5.5? In TIA you can use the built in system-diagnostic. You can acitvate it in the device configuration/HW-Config of the CPU. In the classic Step7 Profinet-diagnostic should be almost the same like the Profibus-diagnostic, with blocks FB126 Diagnostic package PNIODiag for diagnostic evaluation for PROFIBUS DP and PROFINET IO (STEP 7 V5.x)hope this helps, regards, |
FCK WAR! |
|
Follow us on