10/29/2012 8:43 PM | |
Joined: 3/11/2007 Last visit: 10/21/2024 Posts: 226 Rating: (13) |
How to create popup window with KTP 400-bit when PLC switches from 0 to 1? thanks |
10/30/2012 7:51 PM | |
Joined: 3/11/2007 Last visit: 10/21/2024 Posts: 226 Rating: (13) |
Hello, do you vorreri popup window with ktp 400 and wincc flex v11. You have an example or advice? thanks |
10/31/2012 9:41 AM | |
Joined: 4/24/2006 Last visit: 1/13/2025 Posts: 8804 Rating: (1173) |
Hello, Please inform us, which panel you use? (KTP 400 Basic or KTP 400 Comfort) Have a look at the following link: What are the functional differences between the different SIMATIC panels? (With a KTP 400 Comfort, you can use faceplates.) Best regards, Wizard |
10/31/2012 1:17 PM | |
Joined: 3/11/2007 Last visit: 10/21/2024 Posts: 226 Rating: (13) |
Hi, I use the KTP 400 mono basic |
11/3/2012 10:33 PM | |
Joined: 3/11/2007 Last visit: 10/21/2024 Posts: 226 Rating: (13) |
Hello, thanks for the help. How Call her screen from the plc? |
11/5/2012 9:07 AM | |
Joined: 4/24/2006 Last visit: 1/13/2025 Posts: 8804 Rating: (1173) |
Hello, Here are some options: how do you configure screen selection on a Windows-based operator panel with WinCC flexible via controller job 51? how can you make a screen selection on a Windows-based operator panel via the controller without using a controller job? Best regards, Wizard |
Follow us on