6/10/2015 4:55 PM | |
Joined: 8/27/2010 Last visit: 4/13/2024 Posts: 417 Rating: (37) |
Hi! Please check the following thread and my previous answer there. Hope it helps. |
6/16/2015 9:26 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1050) |
Dear YogendraG, see the following manual on page 144: SIMATIC S7-300 S7-300 Module dataAs you can see in the drawing, you have 4 groups of outputs. For each group you have 8 DO´s with 0,5A = 4A with it´s own power supply(L1+/1M;L2+/2M;L3+/3M;L4+/4M). This is the current which goes through the module to the actors.It also depends on the mounting and the ambient temperature, how much current is allowed per group to be save for overheating.The Current consumption of 110mA +160mA is what the module needs for it self to work.hope this helps,regards, |
Last edited by: mopS04 at: 6/16/2015 9:32:50 AMFCK WAR! |
|
6/18/2015 8:30 AM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1050) |
yes, thats what I think too. The current on backplanebus is cominig out of the CPU, and its voltage is 5V. The terms in the technical data of the module with the current from backplane is only for calculation of the power consumption on backplane bus. You can read it in SIMATIC S7-300 CPU 31xC and CPU 31x: Installation, chapter4.5:
The CPU makes out of its own supply of 24V the 5V and runs the backplanebus. So the current on the backplane is allready within the power consumtion of the CPU. This is one reason why the current of the CPU is stated from 150mA to 750mA, because it depends on what moduls are running on the backplanebus. ---> every current on the backplane is irrelevant for his consumption |
FCK WAR! |
|