7/25/2013 10:32 AM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (307) |
Hi RajD WinCC is perfectly suited for such applications. However you need some ADD-ONs / options along with WinCC. Also it is neitherfeasible nor advised to connect the meters directly to TCP/IP. Ideally you should split the plan into sections . Each section can be provided with a S7 based Controller which will read all the required parameters from that area over MODBUS TCP/IPand provide the same to WinCC on Ethernet network. If it is a large plant ( Which it seems to be considering that there are 1000 meters ), you should use F.O. cable for ethernet communication links with length > 100 meters. Here is a useful link giving details of various options available for Energy Management using Siemens Automation : http://support.automation.siemens.com/WW/view/en/68043160 Hope this helps Cheers Navnag |
There is no such thing as the last bug in a program |
|
This contribution was helpful to1 thankful Users |
7/25/2013 10:59 AM | |
Posts: 1530 Rating: (59) |
Hello RajD, please take a look at this: WinCC with OptionSIMATIC powerrateor SIMATIC B.Data. WinCC also offers Redundancy. Best regards Bizur |
7/27/2013 6:04 PM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (307) |
Hi RajD You would not be able to implement a solution using CPY 317-2 DP ( I understand you have thesealso in stock .. else this does not make sense to me ) !! with Redundancy !! ( Why you need redundancy ? ). anyway you cannot plug CP343 in ET200M racks. It would be much more cost effective to use a no of IM 151-8 CPUs ( With onboard Ethernet ). As regards Using WinCC With Modbus TCP/IP, the following links may be useful for you : ( These are mostely about connecting PAC Meters, but same ideas can bee= extended for other meters too : Simple Introduction into Energy Management with WinCC http://support.automation.siemens.com/WW/view/en/48586219 Representation of measuring values without PLC with WinCC http://support.automation.siemens.com/WW/view/en/47903368 Library PAC3200 V1.2 for SIMATIC WinCC V7.0 http://support.automation.siemens.com/WW/view/en/62069929 http://support.automation.siemens.com/WW/view/en/50564890 http://support.automation.siemens.com/WW/view/en/51771311 You will probably have to use the PCs with WinCC forcapturing data from meters in various sections . However pl check the max no of TCP/IP connections on one WinCC ( Not mentioned explicitly anywhere ). I doubt 1000 meters will be easy to integrate like this. You can transfer the Captured data from the PCs to the servers using OPC built into WinCC. Somehow I am not convinced that this is a good solution. Maybe a better solution would be to use your PCs with MODBUS TCP/IP OPC Server ( Third party ) and run WinCC in the Main Server for displayig data and generting reports. Good Luck Cheers Navnag |
Last edited by: Navnag at: 7/27/2013 6:07 PMThere is no such thing as the last bug in a program |
|
This contribution was helpful to1 thankful Users |