2/1/2018 9:27 AM | |
Joined: 3/2/2007 Last visit: 1/9/2023 Posts: 818 Rating:
|
please note that the motor has a mechanical brake on its shaft, controlled from the drive special output, using a brake relay (6SL3252-0BB00-0AA0). the whole control is done with the following items. 6SL3054-4AG00-2AA0-Z E01+F01 , SINAMICS SD-CARD 512 MB empty E01: LICENSE G120 EXTENDED FUNCTION EPOS F01: 1 X SAFETY LICENSE DBSI 6SL3246-0BA22-1FA0 , SINAMICS G120 CONTROL UNIT CU250S-2 PN INTEGRIERT PROFINET SUPPORT OF VECTOR CONTROL, EASY POSITIONING EPOS VIA EXTENDED FUNCTION LICENSE 4 CONFIGURABLE DI/DO, 6 DI (3 F-DI), 5 DI, 3 DO (1 F-DO), 2 AI, 2 AO SAFETY INTEGRATED STO, SBC, SS1 FURTHER SAFETY FUNCTIONS VIA EXTENDED SAFETY LICENSE ENCODER: D-CLIQ + HTL/TTL/SSI, RESOLVER/HTL VIA TERMINAL PROTECTION IP20 USB- AND SD/MMC-INTERFACE thank you |
... thank you ... |
|
2/2/2018 6:50 AM | |
Joined: 6/28/2017 Last visit: 12/20/2022 Posts: 661 Rating:
|
Hi there,
An unexpected turn and now, by a lucky chance we've learned that you going to use separate power supply.
So I created separate topic. Here is a link to: dynamic braking behavior. Msorich |
Last edited by: Msorich at: 2/2/2018 6:52:15 AMLast edited by: Msorich at: 2/2/2018 7:42:10 AMLast edited by: Msorich at: 2/2/2018 12:01:41 PM |
|
Follow us on