Industry Online Support
Technical Forum
4/16/2012 4:46 PM | |
Posts: 30 Rating: (1) |
Hi. I have a 315-2PN/DP CPU and with profinet I concted it tomy dist IO ( I got IM153-4 ). Beside IM153 I have few DIx32 (321-1BL00-OAAO ). I even use 195-7HB00-0AX0 between mine IO:s to the right, soit will bepossible to change IO module while PLC is running. I download my application to CPU and when I am going online in my HW, I can see that CPU have establish connection to my IM153. When I am looking at "module information " for my IO it says: "Module configured, but not available Preset/Actual mismatch: (inserted and configured module types are not the same) - Expected type:IO device (6ES7 321-1BL00-0AA0) - Current type:Not available" It means that IO is "not alive". ´So I guess something must be wrong wiyth Power supplay to my DI . I fount this on internet: http://support.automation.siemens.com/WW/llisapi.dll/csfetch/8859629/s7300_module_data_manual_en-US_en-US.pdf?func=cslib.csFetch&nodeid=10072094&forcedownload=true see page 69 for connection drawing of 1BL00 According to this manual my DI not need any power supplay att all? But whay is no diod lighting on my DI? Why should otherway ModuleInformation say that there is no module att all? Shall Supplay Power go throu this Hot Swap module195-7HB00-0XA0 instead? |
Follow us on