Industry Online Support
Technical Forum
2/10/2012 3:10 PM | |
Joined: 8/31/2010 Last visit: 9/21/2023 Posts: 1499 Rating:
|
Hello Manish, Check this for LEDs - Operator Controls and indicatorsfor your CPU. For IO device related issues, the corresponding BFx will glow and you can refer the corresponding OB. |
Like it? Rate it! |
|
2/20/2012 6:29 PM | |
Joined: 8/31/2010 Last visit: 9/21/2023 Posts: 1499 Rating:
|
Hello Manish, Check the below URLs for basics on configuring the CPU and the IO-device * Configuring the PROFINET interface in a S7-300 PN CPU * Configuring an ET 200S as PROFINET IO device BF1 and BF2 denotes that both the configured MPI/DP and PROFINET networks are having problem. If you have configured the S7-300 PN CPU with an IO-device, then you must have that IO-device working fine. Only then the "Bus Fault" will not glow. What are the other devices you connect in MPI/DP network? |
Like it? Rate it! |
|
Follow us on