3/28/2016 4:41 AM | |
Joined: 9/27/2006 Last visit: 3/25/2023 Posts: 11995 Rating:
|
Hello Learnee; The number of tags available on a TP 1200 Comfort is 2048, it is not expandable. You can locate this information in section 8.8 (Scope of Function with WinCC) of the following manual: SIMATIC HMI HMI devices Comfort Panels https://support.industry.siemens.com/cs/ww/en/view/49313233 These are external tags, or process tags, defined in the glossary of the same manual as a tag interconnected with the PLC. Internal tags (not connected to the PLC) are not counted. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 3/28/2016 4:46:07 AM |
|
This contribution was helpful to
2 thankful Users |
Follow us on