4/19/2022 9:51 AM | |
Joined: 7/8/2019 Last visit: 3/27/2024 Posts: 1 Rating: (0) |
The preinstalled OS on StarterKit not working. FS:02 Version |
4/19/2022 10:19 AM | |
Joined: 4/28/2015 Last visit: 3/23/2024 Posts: 3345 Rating: (377)
|
Hi, is the Example Image pre-installed on the provided SD card? If this is the case, I guess the V1.1.1 is pre-installed, which does not work with IOT2050 Basics FS:02. You need to flash the Example Image V1.2.2 to the SD card. I will check with product management what the provided SD card contains and that this needs to updated if it was V1.1.1. Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
Follow us on