1/16/2012 7:32 PM | |
Joined: 4/22/2010 Last visit: 11/18/2024 Posts: 5697 Rating: (715) |
Hello Tommy, Have you any idea about the range you have to work with? Will it be 0 to 10 bar or up250 bar? What's the medium, gas or fluid? You can have a look here to see how many kinds off pressure transmitters there are: http://www.sensorsone.com/ Regards, Marcjan |
Last edited by: Marcjan at: 1/16/2012 7:43 PMLast edited by: Marcjan at: 1/16/2012 7:36 PMProblem solved? |
|
This contribution was helpful to1 thankful Users |
1/16/2012 10:34 PM | |
Posts: 151 Rating: (8) |
Hi Tomy Master, You are on the Siemens forum , in this link you will see that Siemens has a full range of pressure transmitters: http://www.automation.siemens.com/w1/automation-technology-pressure-measurement-18603.htm#lb-43 Good luck, SonicRanger. |
Last edited by: SonicRanger at: 1/16/2012 10:36 PMLast edited by: SonicRanger at: 1/16/2012 10:36 PM |
|
1/17/2012 6:00 PM | |
Posts: 74 Rating: (3)
|
Hello Tomy Master You don't have enough information to help you make a good choice. I would suggest you go to the Life Cycle portal here https://www.pia-portal.automation.siemens.com,select your language of choice and click on the graphic under Guided Section. This willassist you with the correct selection, or at minimum, narrow down the selection. Concerning a pressure reducing regular, this is not a pressure transmitter. I would suggest you contact your local Siemens representative for a model they may carry. A local contact can be found by clicking the Contacts Worldwide in these Forums. Regards Toppie [ |:) |
1/22/2012 5:16 PM | |
Posts: 64 Rating: (2) |
I do not believe Siemens has any pressure switches in their instrumentation lineup. Common manufacturers are Wika, Ashcroft and United Electric. |
2/24/2012 4:57 PM | |
Posts: 1 Rating: (0) |
Hi, Tomy, There's a specification page at http://www.globalspec.com/learnmore/sensors_transducers_detectors/pressure_sensing/pressure_sensors_instruments that you can use to search for units by type, range, features and so on, which makes it much easier to compare what different manufacturers offer. Best of luck. |
Follow us on