5/19/2014 3:09 PM | |
Joined: 7/7/2010 Last visit: 1/27/2023 Posts: 13080 Rating:
|
I have not had great success with the tool either. One thing I did do was to force my LAN adapter to be in the same subnet as what I am making the PLC. Also, not sure if having the plc in RUN will allow the address change. Should stop the plc, then change the ip address. If you do not have luck and need the PST to work, you can refer to Support Request |
science guy |
|
5/19/2014 3:48 PM | |
Joined: 10/22/2008 Last visit: 12/14/2022 Posts: 355 Rating:
|
LAN adapter is in the same subnet. When the plc is in the stop mode still PST gives before mentioned alarm. |
5/19/2014 4:33 PM | |
Joined: 8/31/2010 Last visit: 2/3/2023 Posts: 1498 Rating:
|
Hello Oscar_83PL, Have you even came across this tool? - How can you change the IP address of an S7-1200 without using STEP 7 Basic? |
Like it? Rate it! |
|
5/19/2014 4:39 PM | |
Joined: 7/7/2010 Last visit: 1/27/2023 Posts: 13080 Rating:
|
Thanks Ganes10 for posting about the specific to s7-1200 tool. That has worked well in the past for me as well. What makes me think the PST4.1 should also work for s7-1200 is the ability to filter on just s7-1200 devices in the PST4.1 filter options. Why put the option to filter on something it has no chance of making work? Regardless, your post will help the original poster with the problem at hand. |
science guy |
|
Follow us on