10/7/2015 5:08 PM | |
Joined: 6/3/2014 Last visit: 1/17/2023 Posts: 660 Rating:
|
Hi, I hesitated posting this, because it's not the easiest solution and more of an idea:
Basically it's a secondary log and the printing of it is triggered by the normal data log. Would be so much easier with messages and recipes.
Another way would be a kind of windows-based script, which is triggered for example by a change in system time and which would print a certain file in a certain location. Then the only thing you have to do in WinCC is copying the logfile to that path and rename it. But I can't help you with applications for Windows CE in C or similar... Or you could archive your data on a pc instead of on the panel. Maybe there you have it easier to integrate automatic printing: https://support.industry.siemens.com/cs/ww/en/view/92346478 |
Last edited by: H.J. at: 10/7/2015 5:15:40 PM~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ★ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ ~ |
|
9/30/2016 7:46 PM | |
Joined: 9/2/2012 Last visit: 6/15/2023 Posts: 711 Rating:
|
Dear Jens, Thank you for the code provided. I am looking for a report generation in PDF format for "Audit" in comfort panel with TP1200. Do you have a script for that ? I havent tried the script that you have posted earlier, but seen your post as below "Can you share the datafile you want to print? The format of the file is attached for your reference. I can get the data log of audit in rdb/unicode txt/csv format. from that i need to make pdf report in day wise and save to storage medium connected. suggestions are welcome !!! AttachmentAuditTrail0 - Copy.zip (902 Downloads) |
|
|
Follow us on