7/22/2009 9:37 AM | |
Joined: 8/8/2008 Last visit: 4/24/2024 Posts: 78 Rating: (4) |
Many Thanks. I have only every used S7 and now I am having to ''STEP'' back in time and use S5 for a project. |
7/23/2009 2:29 PM | |
Posts: 133 Rating: (9) |
Hi Dave Do you have an email address. I tried uploading a step by step guide to printing in Step 5 but I am havving difficulty uploading the PDF file. |
5/21/2010 12:46 PM | |
Joined: 3/21/2006 Last visit: 4/25/2024 Posts: 10228 Rating: (1181)
|
Hello, SIMATIC S5 STEP 5 PRINT Best regards, Hristo Mihalev |
This contribution was helpful to2 thankful Users |
10/21/2018 2:33 PM | |
Joined: 12/18/2014 Last visit: 4/28/2024 Posts: 32896 Rating: (4067) |
Hello 820T, try this. AttachmentSTEP5_Print.zip (256 Downloads) |
This contribution was helpful to1 thankful Users |
10/21/2018 4:18 PM | |
Joined: 12/18/2014 Last visit: 4/28/2024 Posts: 32896 Rating: (4067) |
And STEP5 is so old, so I have not worked with it for years. Do you have the manual for Step5 V7.2? |
10/21/2018 6:16 PM | |
Posts: 51 Rating: (0) |
You Sir are a HERO :) I will go to the workshop and try to do just that - thank you so much . . . .a few minutes later . . .I hope these are the correct files :) Its actually a 'RAR' file but I've renamed it ZIP to be able to upload it Attachment820T.zip (197 Downloads) |
Last edited by: 820T at: 10/21/2018 6:44:43 PM |
|
10/22/2018 11:06 AM | |
Posts: 51 Rating: (0) |
Thank you, but I have managed to fathom it out and produced a .PDF - the attached is just the main program block PB202 Next task is to annotate it with labels for the inputs and outputs that I know from the circuit diagram. AttachmentPB202.pdf (196 Downloads) |
Follow us on