2/19/2015 1:50 PM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating: (2149)
|
Hello xxirokxx, there are two possibilities: 1. You create a layout with an Hardcopy-Object, here can you configure printing the whole screen, or a part of it. Then you create a printjob for this layout. The printjob can you execute from the button in the WinCC-Runtime via a C-script with the function "RPTJobPrint". 2. You write C-script using PrtScr.exe There are some FAQs for it: https://support.industry.siemens.com/cs/ww/en/view/22055343 https://support.industry.siemens.com/cs/ww/en/view/21606152 Regards Georg Berghof |
PS: If this post did really help you, you may use the Rate-button |
|