11/27/2012 5:33 AM | |
Posts: 22 Rating:
|
Dear Expert, Thanks for reply. But i just wanna to ask one more question that the in programing of CPU 315-2DP, when we put the value in db in fb104(Printing Block) that would be automatically connected to string output ..? or we should have to initially that data with db..? here i attached the some program file.please check it. So, please reply on this quote coz of i am in confusion that what should i have to do...?!!
AttachmentAttachment pdf.pdf (170 Downloads) |
11/27/2012 10:55 AM | |
Posts: 3093 Rating:
|
Hello Monik, when you are intending to use P_PRINT I recommend to start with the sample in the Getting Started manual. When the variable is a string, you must set the offset of the variable to 2, as the first two bytes of the string include the length information of the string. Regards, Kaulquappe |
Follow us on