2/1/2017 10:00 AM | |
Posts: 50 Rating:
|
Hello We would like to hear from any one, who has successfully used a post-of-sale (receipt) printer with endless paper to print Report of TP700 Comfort via USB/ Ethernet. The problem is not so many printer's producers develop driver to the HMI. We found on http://star-emea.com/siemens-panels/ the printer Star TSP743II has driver to TP700 but when trying to transfer the driver, using SIMATIC Prosave V14.0.0.0 . we cannot find the driver!? (We followed the guide onhttps://support.industry.siemens.com/cs/de/en/view/11376409 and use SIMATIC Prosave V14.0.0.0.) A local Siemens' support told me that if Ethernet and PostScript is used, a printer will not need a driver. Did any one has experience with this? Best regards Thien |
2/28/2017 5:55 PM | |
Posts: 648 Rating:
|
Dear Thien Nguyen, I followed the post "Printers for SIMATIC HMI Panels": https://support.industry.siemens.com/cs/ww/en/view/11376409 I installed the option ProSave_Opt_1_4_0_0.exe (11428 KB) on my engineering enginge. Made a restart of ProSave. Choose my Panel, give a IP-Address. Then I clicked the tab "Option". Then select the desired printer driver under "Available options". Set "Transfer" mode on the HMI device. Select ">>" on the PC to start the transfer. Follow the ProSave instructions and the instructions which appear on the HMI device. During the installation of the printer driver, a status display appears indicating the progress of the operation. With best regards rh1990 |
This contribution was helpful to
1 thankful Users |
Follow us on