8/23/2011 10:37 AM | |
Posts: 22 Rating: (0) |
Hi, There is a little push button, with a (vertical) text "Reset Batt. + Fan" to reset a Fan alarm (and/or battery failure) Usually the leds willswitch off then after reset,if everything is normal. Otherwise also have a look at the manual: http://support.automation.siemens.com/WW/view/en/1085837 Chapter 4.3 will tell you more... Hope it will help you, Ronald |
This contribution was helpful to1 thankful Users |
8/24/2011 10:03 AM | |
Posts: 3 Rating: (0) |
[quote user="RPvM"]Hi, There is a little push button, with a (vertical) text "Reset Batt. + Fan" to reset a Fan alarm (and/or battery failure) Usually the leds willswitch off then after reset,if everything is normal. Otherwise also have a look at the manual: http://support.automation.siemens.com/WW/view/en/1085837 Chapter 4.3 will tell you more... Hope it will help you, Ronald I had reset the alarm by the "Reset Batt. + Fan" , but the alarm appeared again 6s after a reset was performed.There is now filter mat used here , so I think the air flow is adequate. Thank you for you reply! Kind Regards Luo Jun |
Follow us on