1/17/2007 11:04 AM | |
Posts: 18 Rating:
|
Dear Nemo Thanks for your prompt reply My WinCC is version 6 SP2 but i have tried the samething on SP4 and 6.1 as Well, but same problem is there. I am not using Databridge, I am using standard Connectivity Pack V6.0 SP1 Queries. My OS is MS Windows 2000 Professional The RAM is 512MB, Intel 3GHz Processor. it is not the issue of speed since i have tried it on faster PCs but same bad result due to some bad reason. The relevant WinCC log file is attached from Diagnose Folder Note that when i follow the 4 mentioned stepsstated in my first post, the log file shows as this file shows from following timestamp 255,16.01.2007,15:12:18:109,1007007,1,,(pcname),SCRIPT,ProjectType 1 This is the timestamp when at 3:12 PM local time on 16th Jan,the problem rectified and no delay at 'Set ors1=ocom1.execute'. But before that itried the samething following the same points but of no use. Perhaps you can see in the log file, why? Thanks and regards AttachmentWinCC_SStart_02.zip (31 Downloads) |
Last edited by: Seeker at: 1/17/2007 11:06 AM |
|
1/17/2007 11:11 AM | |
Posts: 3149 Rating:
|
Hi, please attach all logfiles [:D] nemo |
1/19/2007 1:46 PM | |
Posts: 18 Rating:
|
Nemo the whole Diagnose folder is attached Remember the point i made in my initial post about the timestamp when things started working correctly thanks AttachmentDiagnose.zip (65 Downloads) |
1/23/2007 1:34 PM | |
Posts: 18 Rating:
|
Then what should i do? Can anyone elaborate on the four points i mentioned that solve the problem sometimes. |
1/23/2007 11:15 PM | |
Joined: 9/27/2005 Last visit: 11/27/2007 Posts: 1398 Rating:
|
I have come across a similar problem. Unfortunately the only resolution we found was to completely wipe the machine and reinstall everything - Windows, drivers and WinCC ! I second Nemo's suggestion and recommend you open a Support Request. The hotline may be able to help you and are able to escalate issues to the development team if necessary. Salma |
2/6/2007 7:42 AM | |
Posts: 18 Rating:
|
I am sorry but the problem persists Regards |
Follow us on