Industry Online Support
Technical Forum
5/13/2012 3:41 AM | |
Posts: 559 Rating:
|
Dear isurya, If this is the case then you do not have any chances to work without backup of HMI. If it is not possible to get the backup from supplier then you can do one thing. if TP is working with updating values from CPU the You just go to individual screens into and try to find out the tags for all screens by monitoring the values from CPU. If some supplier provides the machine then they are doing good programming like making separate DB for HMI functions. So in your case also if this is available then you just find out that DB & from there you find the tags. I have already put one post to siemens related to this issue. Please see the below link. |
5/13/2012 4:05 AM | |
Posts: 34 Rating:
|
Also,you can directly contact machine supplier. generally in such case they must have programme backup instead of doing it by yourself. |
5/14/2012 7:59 AM | |
Joined: 3/21/2006 Last visit: 2/10/2025 Posts: 10239 Rating:
|
Hello, As I saw HMI pictures (are not complicated) followSolutionFinder'ssuggestion and build a new project. Best regards, Hristo Mihalev
|
This contribution was helpful to
1 thankful Users |
Follow us on