2/6/2015 12:20 PM | |
Posts: 2 Rating:
|
Hi! We also have a problem communicating PAC3200 with SCADA software, over modbus TCP protocol. In our factory we have 19, PAC3200 devices and 3 of them are acting as jklm described, but other 16 seems to not have keep alive period. After 7 days it is not possible to restart communication with device (we were patient ). So keep alive period is probably not set at all. We install powerconfig software but there is not option to set keep alive period. Is there some other option to check if this option is set on device at all? Thanks!
--------------- Split from MODBUS TCP PLC (S7-1200) PAC3200 power analyzer - communication error after power off |
Last edited by: Min_Moderator at: 2/6/2015 4:32:51 PMNew subject after splitting |
|
2/6/2015 9:12 PM | |
Joined: 11/1/2007 Last visit: 5/22/2024 Posts: 36 Rating:
|
Hi, What is the firmware of your pac3200? Try updating your firmware with the latest using powerconfig |
2/9/2015 10:05 AM | |
Posts: 2 Rating:
|
Hi, Thanks for advice. I will upgrade a software. Current version is: SW-REV: V2.2.2 BL-REV: V1.0.2 LP-REV: V2.2.2 |
11/15/2017 2:58 PM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating:
|
New question published by eng_hani_1911 is split to a separate thread with the subject Need help to connect sentron PAC 3200 to 2PCs over scada. Best regards |
Follow us on