6/6/2016 2:26 PM | |
Posts: 2 Rating:
|
Hi, I would like to connect S7-1214C through WinCC v7.2. According to this vedio, I finally succeeded to do so (with WinCC v7.2 upd 7 and Tia v13). But when I reinstalled WinCC v7.2(upd 7) without Tia v13 (without Simatic NET), I could not connect to the PLC any more. I guess it's due to Simatic Device Drivers and Simatic Device Drivers WoW. However, I don't know how to upgrade these two drivers separately 'cause it came out "This shared component cannot be used alone!" (I don't want to install Tia V13). OS: Windows 7 ultimate x64 Could anyone help me. Thanks. |
Follow us on