3/27/2012 11:33 AM | |
Posts: 3037 Rating: (192)
|
Hello, Do you checkthis with a new project? You can use the exampple of faceplate in the following link? How do you create a WinCC flexible faceplate? Can you see this faceplate? Tweety |
3/29/2012 5:23 PM | |
Posts: 133 Rating: (2) |
Hello Tweety yes opening that project i can see the faceplate(furnace)in the library (like it should be correct) |
3/30/2012 7:17 PM | |
Posts: 133 Rating: (2) |
i was trying to create a faceplate but after command "create faceplate" i don t see anything in the library |
4/2/2012 11:33 AM | |
Posts: 3037 Rating: (192)
|
Hello, I can create a faceplate with WinCC flexible 2008 SP2 Update 13. You should reset WinCC flexible with the following link. How can you reset WinCC flexible to the original status of the last installation? Can you post a screenshot for your behaviour? Tweety |
4/11/2012 12:44 AM | |
Posts: 133 Rating: (2) |
Itried to reset winccflexible but it doesnt works |
4/11/2012 10:26 AM | |
Posts: 3037 Rating: (192)
|
Hello, Can you post a screenshot for your behaviour? Which Version of WinCC flexible do you use exactly? Tweety |
4/16/2012 11:33 AM | |
Posts: 133 Rating: (2) |
Winccflexible 2008 SP2 |
4/17/2012 10:45 AM | |
Posts: 3037 Rating: (192)
|
Hello, You have forgotten a screenshotof your behaviour. screenshot Can you create a faceplate at another panel? For example MP277 Tweety |
4/19/2012 3:53 PM | |
Posts: 133 Rating: (2) |
In the attached example i would create a faceplate with 2 I/O fields and 1 I/O graphic field, but in the library i don t see anything; i tried with another pc with the same Winccflexible version and a project with "pc runtime" and it works!
Attachmentscreenshot.zip (51 Downloads) |
Last edited by: O_Moderator at: 4/19/2012 5:42 PM |
|
Follow us on