8/25/2016 12:07 PM | |
Posts: 5 Rating:
|
Hello all, I have the same problem with communication between PLC and WinCC runtime. on the field i have one PLC CPU315-2PN/DP, two TP1200 and one Runtime Advanced. For the TP panels communication works without any problem, but when i put new connection for the Runtime scada, i receive error with communication. When I create new connection, i didn't get the 'station','partner','node' name like on TP panels.. I tried with mode project, also changing the PG/OP interface, but without any positive result. I attached few pictures with problem. IP addresses are good, also the devices are on same network. Also PLC have CP 343 card, i tried to change network to CP card, but unfortunately without any success ... Also i take a look on some examples what i found on net, and make everything like on these sample, but also without any success. Before these project i made one with step7 and TIA runtime without any problems, the only different is that PLC program is now made in Tia ... ps. i'm using Tia V13SP1 update8 Probably you have some solution have to solve these problem .. Thanks in advance, ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 8/25/2016 3:16:43 PMNew subject after splitting |
|
8/25/2016 9:48 PM | |
Posts: 5 Rating:
|
Hello, Sorry, now i tried the procedure what you wrote before, and works properly, Thanks for help, Best regards, Elvis, |
10/25/2016 10:24 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4785 Rating:
|
New question published by Dnakul is split to a separate thread with the subject Problem in Downloading or going Online to IM154. Best regards |
11/4/2016 1:37 PM | |
Joined: 8/21/2014 Last visit: 12/1/2023 Posts: 740 Rating:
|
New question published by electrons is split to a separate thread with the subject Communication failure on starting runtime. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on