1/7/2015 6:41 PM | |
Posts: 17 Rating:
|
DEAR SIEMENS, I am working in a project, where i need to cmmunicate the pac 3200 (Multimeter) with the S7-314c 2PN/DP through profibus network. I have made the hardware configuration with node address of 3 and same address is set in the pac meter 3200. In the pac meter display PGM_FAULT is showing and red light is constantly blowing at the back side of the DP adapter. I tried with both the gsd files available in the forum (GSD-DPV0_19_11 & GSD_PAC3200_V24 ). But, same fault is occurring. As per siemens manual, the above fault is due to the wrong usage of GSD file. Can any one provide me the exact GSD file for the pac meter 3200. Its very urgent, please response as soon as possible. Thanks in advance. Narayanamoorthy
AttachmentERROR MSG.zip (71 Downloads) |
Last edited by: Narayanamoorthy at: 1/8/2015 8:24 AMLast edited by: Narayanamoorthy at: 1/7/2015 6:45 PMLast edited by: Narayanamoorthy at: 1/7/2015 6:42 PM |
|
1/12/2015 4:37 PM | |
Posts: 98 Rating:
|
Hello, here you find the latest gsd Files for PAC3200: ->http://support.automation.siemens.com/WW/view/en/27552047
|
Follow us on