5/6/2012 10:22 AM | |
Joined: 7/8/2009 Last visit: 8/5/2024 Posts: 1976 Rating:
|
Perhaps How is a routing established from one PG via a PROFIBUS interface through a SIMATIC station to SINAMICS G120/G120D frequency inverter via a PROFINET interface? will help you to identify whats wrong Regards Devesh Vithani |
I dont Like people driving Fast, thats the reason I overtake them ;) |
|
5/9/2012 11:13 AM | |
Joined: 10/11/2006 Last visit: 1/22/2025 Posts: 5985 Rating:
|
Hello, as the new generation of theG120 CUs with -2 is used the routingdoes only work if theCPU supports the Dataset Routing. Please see the following FAQ: http://support.automation.siemens.com/WW/view/de/55684745 If a CPU 314C is used it must have a FW ≥3.3 so that the routing to the G120-2works. |
With best regards, |
|
5/11/2012 8:09 AM | |
Joined: 5/21/2008 Last visit: 1/27/2025 Posts: 92 Rating:
|
thanks a lot for your valuable help |
Follow us on