6/4/2013 7:38 AM | |
Joined: 10/7/2005 Last visit: 6/9/2023 Posts: 2969 Rating:
|
Hello GOWDA it seems you are still battling with the same network that gave you problems in the thread PROFIBUS COMMUNICATION ERROR. As such I suggest you follow the advise that you were given in that thread (e.g. study and follow the Design and Installation guidelines from www.profibus.com, check your Network with a Profibus Analyzer etc.). It'll also be much appreciated if you could provide feedback in this and the other thread once you fixed the issue as it may help other users in the future who may have similar problems. I hope this helps |
Cheers |
|
6/6/2013 7:35 AM | |
Posts: 7 Rating:
|
Dear Gowda, Check profibus cables & termination properly at all nodes & make sure that all the drives are working fine. |
Follow us on