8/1/2009 9:31 PM | |
Joined: 12/22/2006 Last visit: 1/25/2022 Posts: 1742 Rating: (309) |
Hello, 1) FDB1 ==> Error in DB 1 Data block DB 1 contains the list of digital inputs/outputs (P peripheral with relative byte addresses from 0 to 127) and the interprocessor communication (IPC) flag inputs and outputs that are assigned to the CPU.
user error, e.g. overwriting system RAM with a block transfer or similar (when a system error is marked, a four-digit hexadecimal number/error code appears at the bottom edge of the screen - refer to RS 75 in Chapter 8). |
Last edited by: edr at: 8/1/2009 9:48 PMLast edited by: edr at: 8/1/2009 9:41 PMLast edited by: edr at: 8/1/2009 9:38 PMBest regards |
|
This contribution was helpful to1 thankful Users |
2/2/2010 5:46 AM | |
Posts: 27 Rating: (1) |
Thanks, problem is solved.Power supply of one of the chassis was faulty. |
Follow us on