2/25/2016 5:10 AM | |
Posts: 21 Rating:
|
Hi, I am using TIA V12. I created a PLC 'user_data_type' (UDT) and I dragged and dropped it in the project library to create the 'user_ data_type' there. It created something but its not 'user_data_type'. It says its [Type version] in its properties as opposed to [user_data_type] (see attached pics). Also this created 'type' is not available to be used in the faceplate 'properties'. I am forced to create a new 'user_data_type' (or HMI UDT) in the project library which is not connected to any PLC 'user_data_type'. So, I have to manage both PLC 'user_data_type' and the project library 'user_data_type', maintenance work is two folds. What I should be able to do is to What am i doing wrong here? Is that limitation of TIA v12 that I am using? How can I make a PLC 'user_data_type' appear in the property interface tab of faceplate?
AttachmentProject Library UDT.zip (47 Downloads) |
Last edited by: Sabeeh at: 8/10/2016 6:26:28 AMLast edited by: Sabeeh at: 8/10/2016 6:51:15 AM |
|
Follow us on