4/8/2021 1:09 PM | |
Joined: 4/28/2015 Last visit: 3/23/2024 Posts: 3345 Rating: (375)
|
Hi, seems you are not the only person having this issue. There are two issues already on github related to that (#54 and #108). #54 seems to be solved with a current build from the github sources. I have never seen this happening with my IOTs using the Example Image V1.0.2. Are you using this version or a custom-build one? Best regards! |
Not working for IOT2050 support anymore from March 1st, 2024. |
|
This contribution was helpful to2 thankful Users |