5/31/2021 4:00 AM | |
Joined: 9/20/2016 Last visit: 11/29/2023 Posts: 11 Rating:
|
What I want is to show the reading of a light ambient sensor, while it range is 0-65535 or 0-100000. Although the resolution is only 1000, I cannot show additional zero in LWE. ixo I have upload both project that able and unable to increase the size of trend view to over 300x300, please check the trendview page. Also, an additional question, regarding both uploaded project, I still cannot change the setting in IOT thing table after I have delete nearly all object in the project, it just say the selected IoT things are referenced, and cannot modified or deleted. What should I do to unlock the IoT Table. AttachmentAble_To_Enlarge.zip (140 Downloads) |
5/31/2021 4:01 AM | |
Joined: 9/20/2016 Last visit: 11/29/2023 Posts: 11 Rating:
|
AttachmentUnable_To_Enlarge.zip (146 Downloads) |
6/1/2021 1:07 PM | |
Joined: 12/18/2014 Last visit: 12/6/2023 Posts: 31560 Rating:
|
It seems that the limiting is screensize -50. By a screen of 300 x 300 is the limit 250 x 250. |
Follow us on