6/23/2019 1:38 PM | |
Joined: 1/1/2017 Last visit: 9/9/2023 Posts: 311 Rating:
|
Hello Siwarexi, I'm facing a similar problem regarding 7MH4910 Load Cell calibration. There are 05 nos of Vibro Chargers. I've calibrated all of them keeping maximum load capacity 25000 kgs. Out of the 05 nos, 02 Vibro Charger's are working perfectly. But 03 of them are showing wrong values >3000kgs I'm attaching the backup of the LoadCell calibrations. Please help me as this is the last job pending on Site. The fault coming is ADC Overload..... Also here are my voltage measurement results: 1.: Pin 12 (+) and pin 13 (-) (voltage is VDC) - 2.3 VDC Waiting for your response. Regards OmKris P.S. ------------------------------------------------------------------------------------------ |
Last edited by: OMKRIS2017 at: 06/23/2019 15:17:49Last edited by: OMKRIS2017 at: 06/23/2019 15:18:53Last edited by: OMKRIS2017 at: 06/23/2019 15:38:59Last edited by: The Helping Hand at: 06/24/2019 12:48:07New subject after splitting |
|
Follow us on