6/4/2015 12:55 PM | |
Joined: 9/8/2009 Last visit: 7/17/2023 Posts: 1410 Rating: (153) |
The grenn cable motion-connect is: 2x2x0,22 + 1x2x0,38 Connectors, crimping tools,...etc: www.yamaichi.de IMO, the connector is Y-ConPlug-21 + Y-ConCover-20 on the drive side. |
6/4/2015 3:37 PM | |
Joined: 1/17/2013 Last visit: 9/28/2023 Posts: 39 Rating: (0) |
If i use cat-6 cable for ethernet communication and rj45 for cliq, will i face any problem? |
6/4/2015 4:39 PM | |
Joined: 9/8/2009 Last visit: 7/17/2023 Posts: 1410 Rating: (153) |
That's impossible. Look for Y-ConPlug-21 at www.yamaichi.de or your cable carefuly. You will see that this ain't RJ45 wit 8 pins, but it has two additional pin on top. You can only cut the original in two parts and then solder wires and shield. But, if you need only to connect CU and motor module, then yes, a good ethernet cable will do the job. Still, you have to find out if it is straight or cross-over. |
Last edited by: Marko Bursic at: 6/4/2015 4:42:25 PM |
|
6/4/2015 5:44 PM | |
Joined: 1/17/2013 Last visit: 9/28/2023 Posts: 39 Rating: (0) |
Can anyone give me the layout of the pins number and connecting cable color code? |
6/5/2015 8:53 AM | |
Joined: 6/30/2009 Last visit: 9/12/2024 Posts: 9 Rating: (1) |
I would try using a Ethernet cable. |
Follow us on