11/24/2018 1:29 PM | |
Posts: 146 Rating:
|
Hello everyone! I have a similar problem. I have CPU 1511-1 PN and ET200SP distributed IO. I did not configure topology. When I connect them directly everything works ok. But when I connect it over cisco switch it does not work. But I can see ET200SP in accessible nodes and I can change its device name and ip address. On this cisco switch CPU 1511-1, ET200SP and many other plcs are connected and CPU 1511-1 is communicating with them using PUT/GET. Any idea what could be the problem? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/24/2018 7:28:38 PMNew subject after splitting Last edited by: Jen_Moderator at: 11/24/2018 7:30:00 PMEdited headline. |
|
12/6/2018 1:21 PM | |
Posts: 146 Rating:
|
Can anyone help? Is there any setting in TIA Portal to enable this? BR, Milos |
12/6/2018 2:59 PM | |
Posts: 146 Rating:
|
Thank you Cristoph! This is the information I needed. When I go on site I will try to configure switch according to your advice. BR, Milos |
Follow us on