3/3/2012 3:19 AM | |
Posts: 3 Rating:
|
anyone please!!!!!! |
3/6/2012 12:29 PM | |
Posts: 3 Rating:
|
Please can anyone helpme with this? any of the administrators or anybody!!!!? |
3/6/2012 5:48 PM | |
Posts: 1547 Rating:
|
Hello, there are some possible reasons for this. So please check your system in following steps: 1. Check configuration with Simatic NET Tools. How do you configure an S7 connection for a user application via Industrial Ethernet with the SIMATIC NET PC software? 2. Check the dependencies of VFD and Access Point of the Application. Check in Station configuration editor in Simatic NET Start menu that you have assigned the right Ethernet card to the access point you call with "dev_name". CH_H1_1: for example. If this is right disable the second network adapter inWindows and try again. If you use TCP you have to assign the TCPentry. If you use Mac address you have to choose ISO entry. The name of configured application in NCM will be the return of your function call S7_get_VFD. Default is "Application" 3. Refer also readme file of SIMATIC NET CD. There are some hints for SAPI S7 Programming interface (but your part is note mentioned there) |
Follow us on